{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is a ZB..W06 ?
Issue:
Identifying an incomplete part number for a light module

Product Line:
Push Buttons and Operator Interface

Environment:
XB2 ZB2 22 mm operators

Resolution:
This is just the general designator for an older 22mm chrome push button direct supply light module assembly with contact blocks and mounting base . A complete number indicates type and number of contact blocks and if bulb of whatever voltage is included . ( ie. a ZB2BW061120V has 1 NO contact and 120v bulb )

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.