Issue:
Product Design Features
Product Line:
QO Three Phase Load Centers
Environment:
Main Breaker
Cause:
Application
Resolution:
The QBL main breaker will physically mount in the load centers, BUT it is not listed on the short circuit current rating table that is supplied in the load centers. Because the QBL is not listed, the installation could violate the NEC, so this is not recommended or warranted.
CTA-ID : 2028524
Product Design Features
Product Line:
QO Three Phase Load Centers
Environment:
Main Breaker
Cause:
Application
Resolution:
The QBL main breaker will physically mount in the load centers, BUT it is not listed on the short circuit current rating table that is supplied in the load centers. Because the QBL is not listed, the installation could violate the NEC, so this is not recommended or warranted.
CTA-ID : 2028524