{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Does the J250R circuit breaker enclosure contain hub provisions in the top endwall?

Issue:
Product design features

Product Line:
Circuit Breaker Enclosures

Resolution:
The J250R is provided with the Series A-L hub opening in the top endwall for use with the Series A-L hub sizes. The catalog numbers of the Series A-L hubs are as follows;
2.0 inch - A200L.
2.5 inch - A250L
3.0 inch - A300L
3.5 inch - A350L
4.0 inch - A400L
In order to use the Series A hub sizes, 1 inch through 2.5 inch, it will require the use of the hub adapter plate, AAP. The bottom endwall, the bottom sidewalls, and the bottom back wall of the J250R does not contain hub provisions, but comes standard with a knockout pattern of C, E, F, G, and H.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: