Issue:
Product Design Features
Product Line:
QO load centers
Resolution:
This riser panel has the interior shifted to the left (panel oriented with main lugs at top).
This restricts branch breakers on the LEFT side of the interior to 30 A max. (DF, CAFI, GFI inclusive).
Maximum branch breaker size on the right of the interior (panel oriented with main lugs at top) follows:
(x) - indicates all suffixes
Product Design Features
Product Line:
QO load centers
Resolution:
This riser panel has the interior shifted to the left (panel oriented with main lugs at top).
This restricts branch breakers on the LEFT side of the interior to 30 A max. (DF, CAFI, GFI inclusive).
Maximum branch breaker size on the right of the interior (panel oriented with main lugs at top) follows:
(x) - indicates all suffixes
Model Number | Max. Breaker |
---|---|
QO11224L125WG(x) | 100 A |
QO12030L125WG(x) | 100 A |
QO13040L200WG(x) | 125 A |
QO124M200WG125(x) | 125 A |
Released for:Schneider Electric Canada