{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What main breaker frame sizes are used in the HCR548612U interior?

Issue:
What size main breakers can be used in the HCRU 1200A I-line panel?

Product Line:
Panelboards

Environment:
I-Line HCR

Cause:
Selection

Resolution:
This accommodates a branch-located main breaker; either an old NA, NC, or NX  or newer Powerpact P frame (PG, PJ , PL ,PGC , PJC , or PLC ) or Powerpact R frame (RGC , RJC, or RLC ) .


Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: