{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What tenant circuit breakers are available for the 200 A MP, MPR, and MPH Meter-Pak meter centers?

Issue:
Product Design Features

Product Line:
Meter Pak metering

Resolution:
The 200 A MP, MPR, and MPH Meter-Pak meter centers will accept type QOM2-MM (10 kAIC) or QOM2-MVH (22 kAIC) tenant circuit breakers, and are available in 100, 125, 150, 175, and 200 A sizes.
Catalog numbers are:
10k AIC rated 22k AIC rated
100 AQOM2100MMQOM2100MVH
125 AQOM2125MMQOM2125MVH
150 AQOM2150MMQOM2150MVH
175 AQOM2175MMQOM2175MVH
200 AQOM2200MMQOM2200MVH

Schneider Electric Canada