{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the LA400F and LA400S circuit breaker enclosures provide the capability to padlock the circuit breaker in either the ON or the OFF position?
Issue:
Product Features

Product Line:
Circuit Breaker Enclosures

Resolution:
The LA400F and LA400S circuit breaker enclosures are provided with the handle padlock attachment HPALM, packaged with the enclosure. This attachment can be field installed on the circuit breaker to provide padlock capability in the ON or OFF positions.

Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: