{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the maximum total length of load wire that can be used with a QO-GFI or QO-EPD circuit breaker?
Issue:
Long load wire run for a QO-GFI or QO-EPD breaker

Product Line:
Miniature Circuit Breakers

Environment:
QO-GFI and QO-EPD Ground Fault Circuit Breakers

Resolution:
The GFI breaker can be used with a 250 ft. maximum circuit length. We do not publish a maximum length for EPD breakers, but the maximum circuit length could be be considerably longer because of the higher GF pickup level.

Schneider Electric Canada