{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the Class 8538 or Class 8539 combination starters seismic rated?
Issue:
What is the form to use for Class 8538 or 8539 combination starters that is seismic rated?

Product Line:
NEMA Contactors and Starters

Environment:
Class 8538 Type S Combination Starter

Resolution:
Yes.  These combination starters (with some exceptions) can be ordered with Seismic qualification using form G20 available in the product selector.

Schneider Electric Canada