{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the replacement Fan Part Numbers for Medium voltage Dry Type transformers made in Milwaukee, or Monroe?

Issue:
What are the replacement Fan Part Numbers and Instructions for Power Cast / Power Dry and Uni Cast Medium voltage Dry Type transformers?

Product Line:
Medium Voltage Transformers

Environment:
Maintanence

Cause:
Replacement parts for 8" , 6W , 120V fan and blades, or 12" , 50W , 120V fan and blades

Resolution:
Note: Confirm the serial number or factory order number, manufacturer location, wattage,  voltage, and Fan Blade diameter before ordering:

For 8" Morrill  6 watt ,120 volt - Fan Motor part# 43500-154-91; 8" Aluminum Fan Blade part# 43500-124-50, or plastic 8" Blade part # 43500-059-41.

For 12" Morrill, 50 watt, 120 volt - Fan Motor part# 43500-124-65; Aluminum Fan Blade (Only option available)  part# 43500-124-67 (12" dia).

A Typical picture of a fan installation:
fan
Note: If parts are not system recognized, please contact MV Transformers support to obtain the ordering information.

See Attached Instruction Bulletin for selecting proper fans associated with the type and KVA of Transformer.

Schneider Electric Canada

Attachment(s)
Fan motor replacement FA Upgrade Inst.pdf [1.28 MB]