{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the catalog numbers for the adder deck screws for 8501 XO relays?
Issue:
Catalog numbers for the adder deck screws for 8501 XO relays.
Product Line:
Relays and Timers
Environment:
8501 Type X Relays
Resolution:
0 to 4 pole adder deck screw is 21101-12401 which is 6-32 x 1 1/4 inches long,
5 to 8 pole adder deck screw is 21101-12681 which is 6-32 x 2 1/2 inches long,
9 to 12 pole adder deck screw is 21101-12781 which is 6-32 x 3 3/4 inches long.

Schneider Electric Canada