{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Can the control coil on the control module of the Tesys U-Line starter be changed?

Issue:
Replacement Control Module coil on the Tesys U Starter

Product Line:
Contactors and Starter - IEC

Environment:
Tesys U Starter

Resolution:
No the coil itself is not replaceable. However you can change the control voltage by simply order a replacement control unit with the desired control voltage code.

Schneider Electric Canada