Issue:
Product Design Features
Product Line:
Load centers and circuit breaker enclosures
Resolution:
The QOM2 breaker allows (1) #4 - 300 kcmil wire and torque is 250 lb-in. or 28 N-m.
NOTE: MAKE SURE TO CHECK THE MAIN WIRE SIZE FOR THE LOAD CENTER THE QOM2 BREAKER IS INSTALLED IN, BECAUSE THE WIRE BENDING SPACE MIGHT BE DIFFERENT ANND WILL NOT ALLOW FOR A 300 KCMIL WIRE
Product Design Features
Product Line:
Load centers and circuit breaker enclosures
Resolution:
The QOM2 breaker allows (1) #4 - 300 kcmil wire and torque is 250 lb-in. or 28 N-m.
NOTE: MAKE SURE TO CHECK THE MAIN WIRE SIZE FOR THE LOAD CENTER THE QOM2 BREAKER IS INSTALLED IN, BECAUSE THE WIRE BENDING SPACE MIGHT BE DIFFERENT ANND WILL NOT ALLOW FOR A 300 KCMIL WIRE