{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What are the repair parts for a SC3040M200S, series M02?

Issue:
Repair parts

Product Line:
CSED

Environment:
Repair parts

Cause:
Maintenance

Resolution:
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED BELOW.
The parts listed here are the only parts considered field repairable:
Meter Cover Assembly - 4056171950
Meter Cover Mounting Screw - 4020513002K (This kit contains 10 screws, but only two screws are required to secure the cover)
Utility Pullbox Cover - 4056194550 (Includes cover latch)
Utility Pullbox Cover Sealing Screw - X1299
Load Center Cover Assembly - 4056172050 (Includes hinges and latch)
Load Center Cover Mounting Screws - (2) 2142217101
Dead Front Interior Trim - 4056170001
Dead Front Interior Trim Mounting Screw - 4020513002K (This kit contains 10 screws, but only two screws are required to secure the interior trim)
Load Center Interior - 4056184950 (Does not include main breaker)
Load Center Interior Mounting Screws - (6) 4020510001
Load Center Line Bussing Insulating Shield - 4056171401
Load Center Line Bussing Insulating Shield Mounting Screw - 4020513002K (this kit contains 10 screws, but only two screws are required to secure the insulator)
Main Breaker - QOM2200VH
Main Breaker Mounting Keps Nuts - (2) 2342702001
Main Breaker Mounting Screw - 4020511201
Meter Base - 7329882750 (base only - does not include jaws, see below)
Meter Base Mounting Screw - (2) 2142717200
Meter Jaw - (4) 7329794850
Meter Jaw Mounting Keps Nut - (4) 2342702001
Meter Jaw Blade Guide - (4) 4052761901
Meter Sealing Ring - 2920910001
Line Side Phase Lug - (2) 4025116051
Line Side Phase Lug Mounting Keps Nut - (2) 2342702001
Line Side Neutral Lugs are not field repairable.
NOTE: WIRING DIAGRAM AND LABELS ARE NOT INCLUDED ON THE PARTS LISTED ABOVE

Schneider Electric Canada

Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: