Search FAQs
What are the replacement lugs for the legacy K frame circuit breakers?
Issue:
Field replaceable lug for the KAL circuit breaker
Product Line:
Legacy Molded Case Breakers
Resolution:
The replacement lug kit for K frame breakers is AL250KA, which is a set of 3 lugs. It can accommodate (1) 4 AWG – 350 kcmil Al/Cu per phase.
Field replaceable lug for the KAL circuit breaker
Product Line:
Legacy Molded Case Breakers
Resolution:
The replacement lug kit for K frame breakers is AL250KA, which is a set of 3 lugs. It can accommodate (1) 4 AWG – 350 kcmil Al/Cu per phase.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: