{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is an auxiliary switch available for both the QO and QOB circuit breakers?
Issue:
How to get auxiliary switch in a QO and QOB breaker?

Product Line:
Miniature circuit breaker

Resolution:
Yes, most QO and QOB circuit breakers can be provided with an auxiliary switch accessory. Use suffix 1200 for an auxiliary switch that is open when the breaker contacts are open (1a) or suffix 1201 for an auxiliary switch that is closed when the breaker is open (1b). Suffix 1212 for 1a1b contacts is NOT valid with QO and QOB circuit breakers.

QO arc fault breakers, QO2150, QO2175, QO2200, QOB2150VH, QOB3110VH, QOB3125VH, and QOB3150VH are not available with an auxiliary switch accessory.

Schneider Electric Canada