{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a QO or Homeline 2p GFI breaker be used to feed a 240 V load that does not have a load neutral wire?
Issue:
Will a QO220GFI breaker work with no load neutral wire for a 240vac application?

Product Line:
QO-GFI, HOM-GFI

Resolution:
Yes. Simply terminate the two hot wires on the breaker and leave the neutral lug unattached. The pigtail wire on the breaker should still be connected to the neutral bar in the panel - this is required to power the push to trip/test feature which verifies the status of the ground fault electronics.

Schneider Electric Canada