{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the EDB, EGB, and EJB type breakers be used on 400 Hz systems?
Product Line:
Circuit Breakers

Resolution:
Yes. The thermal derating for all amperages is 0.97. The magnetic rerating multiplier is 2.6. The interrupting rating is 10% of the 60 Hz interrupting rating.
NOTE: NOT UL LISTED

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.