{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What disconnect switches or circuit breakers were used in the pre-Tesys IEC enclosed combination starters?

Issue:
Identify the part numbers of the breakers included in IEC combination starters

Product Line:
Pre-Tesys Combination Starters

Environment:
IEC Combination Starters

Resolution:
The Pre-TeSys devices were supplied with the following:

Fusible Units:
LE1UD09**, LE1UD12**, LE2UD09**, & LE2UD12** = 9421NC2
LE1UD18**, LE1UD25**, LE2UD18**, & LE2UD25** = 9421NC3
LE1UD32**, LE1UD40**, LE2UD32**, & LE2UD40** = 9421ND3

9421NW2 handle assembly and 9421NS16 shaft assembly.

Circuit Breaker Unit:
LE1UD09**, LE1UD12**, LE2UD09**, & LE2UD12** = GJL36015M03
LE1UD18**, LE1UD25**, LE2UD18**, & LE2UD25** = GJL36030M04
LE1UD32**, LE1UD40**, LE2UD32**, & LE2UD40** = GJL36050M05

9421LG8 circuit breaker operating mechanism, 9421NW3B handle assembly and 9421NS16 shaft assembly.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: