{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the difference between the LUS12 and the LUB12?
Issue:
Which power base to use, LUS12 or LUB12?

Product:
TeSys Motor Starters Open Version

Environment:
Tesys U Starter-Controllers

Resolution:
The LUB12 includes self-protecting features that will trip if a short circuit should occur. The LUS12 is strictly a starter base.

Schneider Electric Canada