{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

How deep of an enclosure can the 9422CFT30 cable operator be used in?

Issue:
What is the depth of enclosure that a 9422CFT30 can be used?

Product Line:
Operating Mechanisms and Disconnect Switches

Environment:
Class 9422 Accessories

Resolution:
It is for use in enclosures of up to 24" deep.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: