{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the replacement for an obsolete HCW2353-6 I-Line panelboard interior?
Issue:
Replacement interior for the obsolete HCW2353-6 I-Line Panel.

Environment:
I-Line panelboards

Environment:
Replacement

Cause:
Cross Reference

Resolution:
Use an HCP23596. It has the same amount of branch mounting space and will fit in the old 74`` high box. However, the original trim will not fit; use the current trim with door or
four piece trim shown in the current Digest.

Schneider Electric Canada