{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Are the QO individual breaker enclosures suitable for use as service entrance equipment and are line side barrier kits available?
Issue:
Characteristics of QO CB enclosures

Product Line:
Circuit Breakers

Resolution:
The QO Circuit Breaker Enclosures are Marked on the wiring diagram label "Suitable for use as Service Equipment", However, Square D does NOT offer any Line Side Barrier Kits to meet the NEC. If the Line Side Barrier kit is required by local code authority, the device should NOT be used for Service Equipment. Consider using the enclosed PowerPact
Q-Frame breaker enclosures.

NOTE: The carton Label for the QO Enclosures, that is located on the outside of the carton for the devices states
"Non-Service Entrance Device", So customers should see and read this label before obtaining the device for use in Service Entrance Applications. See below a visual of the carton label wording.

Visual of carton label



Schneider Electric Canada

Explore more
Product:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: