Issue:
Locating the catalog & series number, date code, and UL logo on Square D™ QO™ and Homeline™ Load Centers.
Product Line:
QO and Homeline Load Centers
Environment:
Catalog and Series numbers
Cause:
Product identification
Resolution:
All of today's current design Series 'S', double row interior construction, Convertible load centers, contains an interior label with the catalog number, series number, and date code on it.
1) For the High Amp(150Amp and above), the interior label is located on one of the Main Lug barriers, either to the far right or far left side of the Main lugs, where the incoming supply wires are connected. The interior label is a white label, approximately 1.5" wide x 2.0" long.
NOTE: If the load center is installed, it might be difficult to locate this label by looking straight ahead at the load center interior and might require the person to take a step either to the right or left and look back at an angle towards the Main Lugs to see the label.
2) For the Low Amp(100-125Amp), the interior label is located on the very top of the interior, either on the right or left side.
NOTE: If the load center is installed, it might be difficult to locate this label, because it will be at the very top of the interior surface and it might require the person to use a ladder to view the actual label.

Locating the catalog & series number, date code, and UL logo on Square D™ QO™ and Homeline™ Load Centers.
Product Line:
QO and Homeline Load Centers
Environment:
Catalog and Series numbers
Cause:
Product identification
Resolution:
All of today's current design Series 'S', double row interior construction, Convertible load centers, contains an interior label with the catalog number, series number, and date code on it.
1) For the High Amp(150Amp and above), the interior label is located on one of the Main Lug barriers, either to the far right or far left side of the Main lugs, where the incoming supply wires are connected. The interior label is a white label, approximately 1.5" wide x 2.0" long.
NOTE: If the load center is installed, it might be difficult to locate this label by looking straight ahead at the load center interior and might require the person to take a step either to the right or left and look back at an angle towards the Main Lugs to see the label.
2) For the Low Amp(100-125Amp), the interior label is located on the very top of the interior, either on the right or left side.
NOTE: If the load center is installed, it might be difficult to locate this label, because it will be at the very top of the interior surface and it might require the person to use a ladder to view the actual label.
Released for:Schneider Electric Canada