Search FAQs
What type of fuse is used with switch part number 44036-325-60?
Issue:
Fuse type used with switch part number 44036-325-60
Product Line:
44036-325-60
Environment:
Fuse type
Cause:
N/A
Resolution:
This switch is a 5kV or 15kV, 600A, 40kA, silver plated, upright, manually operated switch with porcelain insulators. It can be used will all types of fuses below 600E ratings.
Fuse type used with switch part number 44036-325-60
Product Line:
44036-325-60
Environment:
Fuse type
Cause:
N/A
Resolution:
This switch is a 5kV or 15kV, 600A, 40kA, silver plated, upright, manually operated switch with porcelain insulators. It can be used will all types of fuses below 600E ratings.
Released for:Schneider Electric Canada
Explore more
Category:
Explore more
Category: