{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the AL600LI5 lug kit be used with an LAL or LHL type circuit breaker?
Issue:
Can the AL600LI5 lug kit be used with an LAL or LHL type circuit breaker?

Product Line:
Circuit Breakers

Environment:
Application

Cause:
Wire size change

Resolution:
The AL600LI5 lug is intended for use with 600 A L-frame breakers only. There is no equivalent lug available for an LA or LH 400A frame breakers.


Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: