{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What fuse type is required for the 8538SC*12/13/14/22/23/24/62/65 combination starter?
Issue:
Fuse Type required for Combination starter size 1.

Product Line:
NEMA and Definite Purpose Contactors

Environment:
8538 Fusible combination starters

Resolution:
This device is configured from the factory to accept Class H, J, K or R fuse types. However, this device is not supplied with Class R rejection pins. If Class J type (applications above 250 volt) fuses are used it will require re-positioning of the fuse base.

Schneider Electric Canada