{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 9038DG Float Switch be converted to "reverse action" in the field?
Issue:
Is it possible to convert in the field the float switches class 9038 type DG to reverse action?

Product Line:
Pressure, Vacuum and Float switches

Environment:
Pressure Switches - Square D™ NEMA,

Resolution:
Yes, you can adjust it to ``reverse action`` in the field (contacts close on liquid rise) by attaching the float rod to the projection farthest from the pivot point.

Schneider Electric Canada