{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a JDA36225 be mounted in an I Line panelboard and/or Unit Mounted?
Issue:
JDA36225 mounted in an I Line panelboard and/or Unit Mounted.

Product Line:
I line circuit breakers.

Environment:
Product features.

Cause:
Product features.

Resolution:
JDA36225 is an I-Line breaker, and can ONLY be used in a I-Line panel. It can NOT be unit mounted or modified.
For unit mounting with cable connections on both ends, use the JDL36225.

Schneider Electric Canada

Explore more
Category:
Articles that might be helpful Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Category: