{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does an 8538SBA22V02S use 250v or 600v fuses?
Issue:
Are there 30A 250V or 600V fuses on 8538SBA22V02S?

Product Line:
NEMA and Definite Purpose Contactors and Starters

Environment:
Type S Fusible combination starters

Resolution:
250v

Schneider Electric Canada