{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a CAFI breaker be used in place of a GFI breaker?
Issue:
Can a combination arc fault breaker (CAFI) be used in place of a GFI breaker (specifically, a class A GFI breaker)?

Product Line:
Arc fault circuit breakers

Resolution:
A standard CAFI breaker cannot be used to replace a standard GFI breaker, as the CAFI breaker does not have class A ground fault protection. A dual function breaker (combination arc fault + class A ground fault) could be used to replace a standard class A GFI breaker.

Schneider Electric Canada