Issue:
What is the isolated ground bar for use with a larger I-Line panelboard, size HCM and larger?
Product Line:
PTLVS - LV Functiona Enclosures
Environment:
I-Line panelboards sold and supported in the USA.
Cause:
Certain applications require an isolated ground bar in circuit breaker panelboards.
Resolution:
For the larger I-Line panels, the panelboard must use a neutral bar, such as HC2SN or HC6SN, which are isolated from ground, and use it as a an isolated ground bar.
What is the isolated ground bar for use with a larger I-Line panelboard, size HCM and larger?
Product Line:
PTLVS - LV Functiona Enclosures
Environment:
I-Line panelboards sold and supported in the USA.
Cause:
Certain applications require an isolated ground bar in circuit breaker panelboards.
Resolution:
For the larger I-Line panels, the panelboard must use a neutral bar, such as HC2SN or HC6SN, which are isolated from ground, and use it as a an isolated ground bar.