{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a 5.0 or 5.0A trip unit be used for ground fault alarm without tripping?
Issue:
How to set up and test ground fault alarm in Micrologic trip units

Product Line:
Molded Case and Air Circuit Breaker

Resolution:
No. Neither the 5.0 nor 5.0A trip units can be used because those trip units do not have the required programming functionality.
To get ground fault alarm without tripping, replace the trip unit with a 5.0P or 5.0H trip unit, add an M2C or IO programmable contact module, and program the trip unit for the alarm.

Schneider Electric Canada