{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can a Model 85 or Model 85A Life-Gard temperature controller be repaired?
Issue:
Life-Guard Controller

Product Line:
Transformers

Environment:
Medium Voltage

Cause:
Maintenance

Resolution:
Neither Square D nor the manufacturer of the Model 85 or Model 85A Life-Gard temperature controllers repairs the controller. However, the following company repairs the controllers.

Solid State Exchange & Repair Co.
4701 Spartan Dr.
Denton, TX 76207
Ph: 940-243-3731

Schneider Electric Canada