{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What are the padlock attachments for Powerpact M, P, and R frame breakers?
Issue:
Powerpact M, P, & R frame padlock attachments: which one will lock on and off?

Product Line:
Molded Case Circuit Breakers

Resolution:
For M, P, and R frame breakers:
  • Use an S32631 for a fixed, lock OFF or ON padlocking device.
    • For factory installation of S32631, use suffix YP.
  • Use an MPRPAF for a fixed, lock OFF only padlocking device.
    • For factory installation of MPRPAF, use suffix YQ.
For M and P frame breakers:
  • Use an S44936 for a removable, lock OFF only padlocking device.
For R frame breakers:
  • Use an S33996 for a removable, lock OFF only padlocking device.

Schneider Electric Canada