{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

What is the catalog number for the replacement handle for the Powerpact M and P frame circuit breakers?

Issue:
Is there a toggle handle replacement for the PowerPact M and P Frame breakers?

Product Line:
Molded Case Circuit Breakers

Resolution:
The handle extension is the only part of the handle available for replacement. It is part number S46998 (S46996 is an option longer handle extension). If the nub under the extension is broken, the breaker has to be replaced.

Schneider Electric Canada