{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Which Tesys overload relays include the W816366180111 spacer?
Issue:
What is the cross for a W816366180111 TeSys overload relay spacer for a LRD22?

Product Line:
IEC Contactors and Starters

Environment:
TeSys™ D Contactors and Overload Relays

Resolution:
W816366180111 is obsolete, replaced by LAD903. The LRD22, LRD32, and LRD35 include this spacer in the carton. The customer must mount it on the relay before installing the overload to the contactor. This support piece provides good stability of the overload on the contactor, mainly while wiring. W816366180111 is obsolete, replaced by LAD903. Anytime the smaller overloads (LRD01 - LRD21 or LRD1508 - LRD1521) are direct mounted to the LC1D25 or LC1D32 contactors, LAD903 will provide stability while wiring.

Schneider Electric Canada