{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Does the SDSB1175 provide protection for sub panels located downstream of the main panel?
Issue:
Does the SDSB1175 provide protection for sub panels located downstream of the main panel?

Product Line:
Surge Protective Devices (SPDs)

Environment:
Maintenance

Resolution:
Certainly! The SDSB1175C offers protection from surges originating from the utility side of the home. It's advisable to install surge protective devices on all downstream panels to safeguard against surges from the loads connected to each panel and from let through surges. The SPD at the main panel may be too distant to respond quickly to internal surge events.

Schneider Electric Canada