{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
If I use a 9421LR1 door mounting operating mechanism with an LAL type breaker, and the breaker trips, will the handle on the door indicate that the breaker has tripped?
Issue:
Identify the operation of the 9421 operating mechanism.

Product Line:
Class 9421 Operating mechanism

Environment:
Square D Operating Mechanisms and Disconnect Switches

Resolution:
The handle will move to a position between On and Off, and this will indicate tripped. There is also a printed indication on the handle bezel for "trip".

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: