{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.

Search FAQs

Are the contacts of a 9001KA2 convertible to NC or 9001KA3 convertible to NO?

Issue:
Can the 9001KA2/3 be field convertible?

Product Line:
Push Buttons and Operator Interface

Environment:
Harmony 9001K/SK

Resolution:
No, the contacts of a 9001KA2 are fixed normally open and the contacts of a 9001KA3 are fixed to normally closed.

Schneider Electric Canada

Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Range: