{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Do the QOMB1, QOMB2, or QOMB3 mounting bases have a DIN rail mounting clip?
Issue:
Product Features

Product Line:
OEM Mounting Bases

Resolution:
These OEM mounting bases do not have the capability of being DIN rail mounted. They are for surface mount only.

Schneider Electric Canada

Explore more
Product:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Explore more
Product: