{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Is the rod only available for the XB4BA*** reset operators?
Issue:
Identify if there's a replacement for the rod of a reset operator

Product Line:
22mm Push Buttons

Environment:
ZB4/ZB5 22mm Push Buttons

Resolution:
No. Reset operator must be purchased as complete assembly.

Schneider Electric Canada

Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.