Issue:
Product Features and Selection for Digital Clock/Timer MCT12BC
Product Line:
Power Monitoring and Control
Environment:
NFPA99, NEC517.160 OR PANELS/LIMS
Cause:
Separate part numbers allow a product to be ordered in component parts, or individual components may be replaced.
Resolution:
Please note that this product is obsolete and has been superseded by the Iso-Gard IGT Dual Clock/Timer. MCT12B, MCTCT, MCTS95135, 53007BB are the components that make up the MCT12BC.
Product Features and Selection for Digital Clock/Timer MCT12BC
Product Line:
Power Monitoring and Control
Environment:
NFPA99, NEC517.160 OR PANELS/LIMS
Cause:
Separate part numbers allow a product to be ordered in component parts, or individual components may be replaced.
Resolution:
Please note that this product is obsolete and has been superseded by the Iso-Gard IGT Dual Clock/Timer. MCT12B, MCTCT, MCTS95135, 53007BB are the components that make up the MCT12BC.
Released for:Schneider Electric Canada