{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
What is the power supply requirement for Micrologic trip units for Powerpact P and R frames and Masterpact breakers?
Issue:
What is the power supply requirement for Micrologic trip units for Powerpact P, R and Masterpact breakers?

Product Line:
Powerpact and Masterpact

Resolution:
The power requirement for all Micrologic trip units for Powerpact P and R frames and Masterpact breakers is 50 mA @ 24 Vdc ±5%, max ripple 1%. Use terminals F2 (+) and F1(-).
Picture showing the wiring diagram of the trip units
For help with Micrologic trip units and modbus communications for Masterpact and Powerpact P and R circuit breakers, consult instruction manuals:
Powerpact P, R, and Masterpact NW, NT Micrologic™ types 2.0, 3.0 and 5.0 Trip Units, see 48049-207-05
Powerpact P, R, and Masterpact NW, NT Micrologic™ 2.0A, 3.0A, 5.0A, and 6.0A Trip Units, see 48049-136-05
Powerpact P, R, and Masterpact NW, NT Micrologic™ 5.0P and 6.0P Trip Units, see 48049-137-05
Powerpact P, R, and Masterpact NW, NT Micrologic™ 5.0H and 6.0H Trip Units, see 48049-330-03

Schneider Electric Canada