Issue:
8903L*1200 or 8903LX*1200, Can they Add One Additional Power Pole?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8903 Type L & LX Lighting Contactors
Resolution:
You cannot add additional power poles onto the 8903L*1200 or 8903LX*1200, it is already at the maximum of 12 poles.
8903L*1200 or 8903LX*1200, Can they Add One Additional Power Pole?
Product Line:
NEMA and Definite Purpose Contactors and Starters
Environment:
Class 8903 Type L & LX Lighting Contactors
Resolution:
You cannot add additional power poles onto the 8903L*1200 or 8903LX*1200, it is already at the maximum of 12 poles.