Search FAQs
What factory modification is required to add shunt trip to the Class 8539 combination starter?
Issue:
What is the form used to add shunt trip to the Class 8539 combination starter?
Product line:
NEMA Contactors and Starters
Environment:
Class 8539 Type S Combination Starter
Resolution:
Use Form Y545. This adds shunt trip feature to any thermal magnetic or Mag-Gard circuit breaker. Voltage of shunt trip mechanism will be the same as the specified controller control voltage. Shunt trip will be unwired unless specified or ordered with Form Y450 (Ground Fault Protection).
Note: Form Y450 is NOT available with Spin-Top designs.
What is the form used to add shunt trip to the Class 8539 combination starter?
Product line:
NEMA Contactors and Starters
Environment:
Class 8539 Type S Combination Starter
Resolution:
Use Form Y545. This adds shunt trip feature to any thermal magnetic or Mag-Gard circuit breaker. Voltage of shunt trip mechanism will be the same as the specified controller control voltage. Shunt trip will be unwired unless specified or ordered with Form Y450 (Ground Fault Protection).
Note: Form Y450 is NOT available with Spin-Top designs.
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: