{}

Our Brands

Impact-Company-Logo-English Black-01-177x54

Welcome to the Schneider Electric Website

Welcome to our website.
Search FAQs
Can the operating handle of a double throw safety switch be padlocked in the ON or OFF position?
Issue:
Lock ON Provisions

Product Line:
Double Throw Safety Switches

Resolution:
Lock OFF:
Provision to lock the operating handle in the OFF position is standard on all double throw safety switches.

Lock ON:
Provision to lock the handle in the ON position is available (subject to local code regulations - consult local authorities for interpretation)

DT and DTU, 30 - 100 A, Series F switches: factory installed standard feature and no suffix needed
82000 and DTU, 200 A, Series E1 and E2 switches: factory installed option only; add suffix 'SPLO' to standard catalog number
82000, 200 A and 400 A, Series E3 and A1 switches: factory installed standard feature and no suffix needed
92000 (Series E or Series T) devices:  factory installed standard feature, no suffix needed
DTU, 400 A and 600 A, Series A__ switches: not available

Schneider Electric Canada