{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
Will inductive proximity switches work on aluminum?
Issue:
Will inductive proximity switches work on aluminum?

Product Line:
Schneider Electric prox sensors sold and supported in the USA.

Environment:
Installation

Cause:
Application

Resolution:
Yes but the range is decreased using aluminum, usually achieving about 40% of the rated range using a standard target made of ASTM A36 mild steel. The one exception is aluminum foil [<0.1 mm] which makes an excellent target. This is due to an obscure principal known as the ``skin effect``. Other possibilities include the XS....KPM40 universal series which detect all metals at the same range and the XS1M18PAS20(D) which are specific for non-ferrous metals.

Schneider Electric Canada

Will inductive proximity switches work on aluminum?
Issue:
Will inductive proximity switches work on aluminum?

Product Line:
Schneider Electric prox sensors sold and supported in the USA. 

Environment:
Installation 

Cause:
Application

Resolution:
Yes but the range is decreased using aluminum, usually achieving about 40% of the rated range using a standard target made of ASTM A36 mild steel. The one exception is aluminum foil [<0.1 mm] which makes an excellent target. This is due to an obscure principal known as the ``skin effect``. Other possibilities include the XS....KPM40 universal series which detect all metals at the same range and the XS1M18PAS20(D) which are specific for non-ferrous metals.

Schneider Electric Canada

Explore more
Range:
Explore more
Range:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Range:
Explore more
Range:
move-arrow-top