Search FAQs
What is the UL E file number for the SDSA3650.
Issue:
What is the UL E file number for the SDSA3650.
Product Line:
Surge Protective Devices (SPDs)
Environment:
Maintenance
Cause:
UL File Number
Resolution:
The two file numbers that apply to this device are as follows:
What is the UL E file number for the SDSA3650.
Product Line:
Surge Protective Devices (SPDs)
Environment:
Maintenance
Cause:
UL File Number
Resolution:
The two file numbers that apply to this device are as follows:
- Surge arrestor UL file E-148456 Vol.1 Sec. 4
- TVSS UL file E-81066 Vol.2 Sec.28
Released for:Schneider Electric Canada
Explore more
Range:
Explore more
Range: