{}

Our Brands

Welcome to the Schneider Electric Website

Welcome to our website.
How can we help you today?
What is the part number for the 1/4 turn fasteners shown in Panelboard instruction bulletins

Issue:
1/4 turn part number from manuals  80043-450-02, 80043-450-03, and 80043-772-01

Product Line:
NQ NF Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
This hardware is not the standard hardware for attachment of hinged trims; therefore, it may be difficult to identify.

Resolution:
Order as a kit part number LP9503. This comes with 4 fasteners per kit.

Schneider Electric Canada

What is the part number for the 1/4 turn fasteners shown in Panelboard instruction bulletins

Issue:
1/4 turn part number from manuals  80043-450-02, 80043-450-03, and 80043-772-01

Product Line:
NQ NF Panelboards

Environment:
UL 67, UL 50, CSA C22.2 No.'s 20-M1989 & 94-M91, NEMA PB1, NFPA 70 Art. 408, Federal Specification W-P-115C Type 1 Class 1 , 2003 IBC, NFPA 5000, ASCE/SE17

Cause:
This hardware is not the standard hardware for attachment of hinged trims; therefore, it may be difficult to identify.

Resolution:
Order as a kit part number LP9503. This comes with 4 fasteners per kit.
 

Schneider Electric Canada

Explore more
Category:
Explore more
Category:
Users group

Discuss this topic with experts

Visit our Community for first-hand insights from experts and peers on this topic and more.
Users group

Discuss this topic with experts

Visit our community and get advice from experts and peers on this topic and more
Explore more
Category:
Explore more
Category: